Skip to main content
REHLKO BRANDS

KOHLER ENERGY - ENGINES SELECTED AS FINALIST IN INAUGURAL NEXT LEVEL AWARDS PROGRAM AT CONEXPO LAS VEGAS

CONEXPO-CON/AGG and the International Fluid Power Exposition (IFPE) have selected as one of the top 10 finalists for the Next Level Awards Program with the KSD engine.

The CONEXPO-CON/AGG Next Level Awards celebrate exhibiting companies that are pushing the boundaries and developing next-level products, technologies and services designed to advance the construction industry.

The KSD, Kohler Small Displacement, is Kohler state-of-the-art engine in the under 19 kW category introduced in 2021. The KSD has already been a symbol of 2022, winning both the Engine of the Year award from Diesel and Powertrain Magazine, and the Engine of the Year under 175 hp award at the Diesel Progress Summit in Chicago.

The KSD features a revolutionary electronically controlled indirect injection combustion system, as opposed to the standard mechanical indirect injection in this category. The engine performance is maximized in every operating condition, with outstanding responsiveness. The remarkable low-end torque values allow the operator to run their equipment at lower engine speed to save fuel. The electronic injection system results in no visible black smoke, and noise and vibrations are minimized.

“We are enthusiastic and honored to be among the top 10 finalists in the Next Level Awards program. It is further recognition of the outstanding work of the KSD team, dedicated to providing customers with the best engine in the 25-hp range” said Vincenzo Perrone, President of KOHLER Energy - Engines. “This is another step that demonstrates Kohler's strong commitment to the industry and continued investment in new engines.”

“We’re excited to recognize these innovative construction products that are taking the industry to the next level,” said Dana Wuesthoff, CONEXPO-CON/AGG show director. “And March 14-16, it will be in the hands of CONEXPO-CON/AGG attendees to determine the Contractors’ Top Choice.”

KOHLER Energy - Engines will be recognized with signage in booth S84406, South Hall 4, so show attendees can vote on-site to determine the Contractors’ Top Choice. Attendees will be able to scan a QR code and vote for their favorite entry.

The KSD was selected by a diverse panel of Associated General Contractors of America (AGC) members. It was judged based on three criteria:

  • Addresses a common industry need in a unique and innovative way. 

  • Benefits the industry across multiple applications for industry wide adoption. 

  • Positively impacts the safety, sustainability, and workforce of the industry. 

Voting will only take place onsite at the show. Registration for CONEXPO-CON/AGG and IFPE is currently 20 percent off with code MEDIA20.

 

About KOHLER Energy - Engines

Kohler has been manufacturing engines for more than a century and has continued to grow its product portfolio ever since its inception to increasingly bring ease and convenience to the lives of end users worldwide. The company offers a comprehensive range of diesel, petrol and gas engines up to 140 hp of power – adopted globally by machine and equipment manufacturers in the most important sectors of industry (construction, earth-moving, agriculture, generators and gardening). For more details, please visit kohlerengines.com.

About Kohler Co.

Founded in 1873, Kohler Co. is one of the oldest and largest private companies in the U.S., based in Kohler, Wisconsin. With more than 50 production plants worldwide, Kohler is a global leader in the manufacturing of engines, generators, kitchens and bathroom furnishings. In addition, it owns and operates two of the finest five-star luxury golf resorts in the world, one in Kohler, Wisconsin and the other in St. Andrews, Scotland. For more details, please visit kohlercompany.com.

About CONEXPO-CON/AGG 

CONEXPO-CON/AGG is the largest construction trade show in North America and the premier event that connects professionals from every major construction sector. Held every three years, CONEXPO-CON/AGG takes the construction industry to the next level by helping construction professionals elevate their industry expertise, experience the newest equipment and products through demonstrations and industry-leading education, make new professional connections, and grow their own marketability within the industry. The next CONEXPO-CON/AGG will be held March 14-18, 2023, in Las Vegas, Nevada. For more information on CONEXPO-CON/AGG, visit https://www.conexpoconagg.com.

About the International Fluid Power Exposition (IFPE) 

IFPE, the International Fluid Power Exposition, is the leading North American exhibition bringing together the fluid power, power transmission and motion control industries. The next IFPE, co-located with CONEXPO-CON/AGG, and located in South Hall, second level, will be held March 14-18, 2023, at the Las Vegas Convention Center. 

Media Inquiries

CONTACT | Public Relations
Chiara Danese
chiara.danese@rehlko.com 

+39 0522 389471

Join Media List 


Kohler

Resilience is reinvention

Kohler Engines is now Rehlko

Follow us on