Skip to main content
REHLKO BRANDS

KOHLER Engines At Hillhead

June 2022 - Everything is ready for Hillhead, the iconic trade show dedicated to the quarrying, construction and recycling industries, that this year celebrates its 40th anniversary. Kohler will be there on June 21-23 with a booth that this year will speak not only to OEMs but also to the rental world.

Today’s engines are increasingly complex. For Kohler, offering the highest levels of technology while ensuring simplicity for the manufacturer is a real mission. For this reason, the undisputed star of this year’s show will be a historic member of Kohler’s KDI line, the 1903TCR Stage V in Power Pack version.

The Power Packs are the ultimate expression of Kohler’s philosophy: advanced technology with compact and efficient solutions. Designed to be integrated into various applications with minimal installation effort, Power Packs possess a quick and easy interface that can significantly reduce customers’ time-to-market due to limited reengineering requirements. The turbo-common rail and various ATS system (Kohler Flex solutions) – which can be engine mounted or chassis mounted – meet the diverse emission needs of OEMs worldwide. Even the most demanding applications are met, thanks to an extensive list of options to choose from, such as PTO’s, air filters, and speed controls. The cooling system is designed and built to work in the toughest conditions, ensuring reliability and quality at the highest level.

The Power Pack line has a power range from 19 to 112 kW. The best-in-class engine for its displacement is the KDI 3404, which offers outstanding performance with a maximum power output of 112 kW at 1800 rpm and a maximum torque of 650 Nm at 1400 rpm.

As with all of the company’s other products, Power Pack solutions benefit from Kohler’s global service network, which boasts 2,000 diesel outlets worldwide and more than 8,000 gasoline outlets with the highest standards.

Hillhead will also be an opportunity to talk about the Kohler Rental Partner Program, an ad hoc project that provides participating rental companies with specific training courses, dedicated discounts for the purchase of original spare parts, and access to all aftermarket documentation. Training meetings are organized with Kohler’s specialized speakers, with in-depth coverage of ordinary maintenance of the various engine families, electronic engine operation, and independent or remotely assisted diagnostics.

The goal of the program is to lower the total cost of ownership that falls on the rental partner, making it more independent and efficient in the management of its fleet, with the intention of decreasing downtime and making vehicles available for rental as soon as possible.

About Kohler Engines
Kohler has been manufacturing engines for more than a century and has continued to grow its product portfolio ever since its inception to increasingly bring ease and convenience to the lives of end users worldwide. The company offers a comprehensive range of diesel, petrol and gas engines up to 140 hp of power – adopted globally by machine and equipment manufacturers in the most important sectors of industry (construction, earth-moving, agriculture, generators and gardening). For more details, please visit kohlerengines.com

About Kohler Co.
Founded in 1873 and headquartered in Kohler, Wisconsin, Kohler Co. is one of America’s oldest and largest privately held companies comprised of more than 40,000 associates.
With more than 50 manufacturing locations worldwide, Kohler is a global leader in the design, innovation and manufacture of kitchen and bath products; luxury cabinetry, tile and lighting; engines, generators, and clean energy solutions; and owner/operator of two, fivestar hospitality and golf resort destinations in Kohler, Wisconsin, and St. Andrews, Scotland. Kohler’s Whistling Straits golf course recently hosted the 43rd Ryder Cup. The company also develops solutions to address pressing issues, such as clean water and sanitation, for underserved communities around the world to enhance the quality of life for current and future generations. For more details, please visit kohlercompany.com.

Media Inquiries

CONTACT | Public Relations
Chiara Danese
chiara.danese@rehlko.com 

+39 0522 389471

Join Media List 


Kohler

Resilience is reinvention

Kohler Engines is now Rehlko

Follow us on