Skip to main content
REHLKO BRANDS

KOHLER Engines Approves Usage Of Hvo In The USA

All Kohler diesel-fueled engines are approved to use HVO in the United States, in line with ASTM D975 standard. This confirmation comes just a few months after European compliance was announced. In February, in fact, Kohler had announced approval to use HVO for all its diesel engines in Europe, in line with the EN15940 standard.

The use of HVO, hydrotreated vegetable oil, whether pure or blended with conventional diesel, does not require any specific engine modifications or upgrades. However, exhaust gas aftertreatment system remains necessary where already provided.

Unlike conventional biofuels that take resources away from agriculture and contribute in part to deforestation, HVO is a renewable fuel that can be produced from various vegetable oils and fats: it is derived from biological waste and, free of fossil-derived oils, is a 100% recycled product. In addition, depending on the raw material used in its production, it leads to a reduction in overall CO2 emissions of up to 90%. Engine exhaust emissions also benefit directly, given the very low sulfur content.

This announcement marks another step toward Kohler's new roadmap, which for the first time outlined its strategy for a more sustainable future at the Bauma Media Dialog in Munich. Among the new pillars of the strategy, alternative fuels are aimed at raising awareness of low-carbon, more economical and logistically manageable fuels. The emphasis, as always, is on innovation and the use of technologies to guide the company toward the green transition, without losing sight of the different needs of OEMs, and keeping engine performance high thus maximizing machine productivity.

About Kohler Engines
Kohler has been manufacturing engines for more than a century and has continued to grow its product portfolio ever since its inception to increasingly bring ease and convenience to the lives of end users worldwide. The company offers a comprehensive range of diesel, petrol and gas engines up to 140 hp of power – adopted globally by machine and equipment manufacturers in the most important sectors of industry (construction, earth-moving, agriculture, generators and gardening). For more details, please visit kohlerengines.com

 About Kohler Co.
Founded in 1873 and headquartered in Kohler, Wisconsin, Kohler Co. is one of America’s oldest and largest privately held companies comprised of more than 40,000 associates.
With more than 50 manufacturing locations worldwide, Kohler is a global leader in the design, innovation and manufacture of kitchen and bath products; luxury cabinetry, tile and lighting; engines, generators, and clean energy solutions; and owner/operator of two, fivestar hospitality and golf resort destinations in Kohler, Wisconsin, and St. Andrews, Scotland. Kohler’s Whistling Straits golf course recently hosted the 43rd Ryder Cup. The company also develops solutions to address pressing issues, such as clean water and sanitation, for underserved communities around the world to enhance the quality of life for current and future generations. For more details, please visit kohlercompany.com.

Media Inquiries

CONTACT | Public Relations
Chiara Danese
chiara.danese@rehlko.com 

+39 0522 389471

Join Media List 


Kohler

Resilience is reinvention

Kohler Engines is now Rehlko

Follow us on